The operator workplace show system is in design mode
The operator workplace show system is in design mode
How can i remove it?
How can i remove it?
Answers
What type of license you've got? If its not a production license and if you are using production features such as operator workplace, faceplates, alarmlist then you will see Design mode on left corner. It is equivalent to license violation pop up but less annoying.
I got this before when I use 800xA system 6.0 at first.
You have to change "Design Phase" to "Production Phase" in software factory.
Also, you can find into "Reference Central Licensing System.
Document No : 2PAA111691-610
You have to change "Design Phase" to "Production Phase" in software factory.
Also, you can find into "Reference Central Licensing System.
Document No : 2PAA111691-610
by chandrakishore Rank: 297 on 7/10/2019 8:11:10 AM | Like (0) | Report
Do you mean that is it in editing mode?
by Abdelmohsen.nasser Rank: 1263 on 7/10/2019 8:16:03 AM | Like (0) | Report
No in design mode it at bottom inthe right of the screen
by chandrakishore Rank: 297 on 7/10/2019 8:17:27 AM | Like (0) | Report
Can you please attach pic of that
by Abdelmohsen.nasser Rank: 1263 on 7/10/2019 8:20:58 AM | Like (0) | Report
I am not in the site now i will attach tomorrow
But it written as same as the `activate windows` when the windows is not activated
Add new comment