How to define ADVANT USER DEFINED library in 800xA?
Hi dear
We have 800xA for advant. We use MB300 uploader - Tab from FCB for upload from source file for upload objects.
after completion all existence standard advant object type (such as AI MB300, AO MB300,...) created in control structure.
But my problem is in advant controller used user defined function (for example MOT10). MOT10 is not exist in object type stucture and for this reason after upload from source file we haven't MOT10 instance in control structure.
My question is How to define user defined function (MOT10) in advant object type?
Answers
A user defined function is a PC element. It will write data to a variant of an existing Database Element - usually an MMCX.
The MMCX elements should all have been uploaded, but the variants used for MOT10 will have no faceplates, graphic elements, object displays etc. You have to build these yourself or have them built for you.
You can contact me off-forum if you do not have someone else who can do this for you.
The MMCX elements should all have been uploaded, but the variants used for MOT10 will have no faceplates, graphic elements, object displays etc. You have to build these yourself or have them built for you.
You can contact me off-forum if you do not have someone else who can do this for you.
Add new comment