Profinet communication of ABB PM591-ETH with Siemens ET200 S (IM151 -3 PN ST) module
Hi all,
I am communicating ABB PLC PM591-ETH with Siemens ET200 S (IM151 -3 PN ST) module through profinet via CM 579 module. I have set parameter setting same as for CI 502 module. But communication is not happening. Is there will be any change in parameter for the Siemens module? Is memory card is required for ET200S module for communication? Need help on this?
Following is the catlog number for siemens ET 200 S module.
Siemens module Cat. No.- IM151-3 PN ST V7.0 (6ES7 151-3AA23-0AB0)
I am communicating ABB PLC PM591-ETH with Siemens ET200 S (IM151 -3 PN ST) module through profinet via CM 579 module. I have set parameter setting same as for CI 502 module. But communication is not happening. Is there will be any change in parameter for the Siemens module? Is memory card is required for ET200S module for communication? Need help on this?
Following is the catlog number for siemens ET 200 S module.
Siemens module Cat. No.- IM151-3 PN ST V7.0 (6ES7 151-3AA23-0AB0)
Answers
This question has not yet been answered.
Add new comment