2 different LDCM modul communicate
Hello Everyone,
I have 2 differential relays but they have different LDCM modul ( long and medium). So is it possible to comminicate each other? And how we can do it?
Sincerly
I have 2 differential relays but they have different LDCM modul ( long and medium). So is it possible to comminicate each other? And how we can do it?
Sincerly
Answers
Despite the fact that both Medium range (MR) and Long range (LR) are using Singlemode 9/125 μm However they are using different wave length whereas MR and LR are using wave length of 1310 nm, 1550 nm respectively.
Also, the optical budget are different as week 20dB and 26 dB which can cause a damage in the receiver of MR side.
Also, the optical budget are different as week 20dB and 26 dB which can cause a damage in the receiver of MR side.
Add new comment