How to delete project from cb and ctrl structure?
Voted best answer
ASO object class xxxx did not implement IAfwAspectSystemObject. Failed to create ASO. Forgot to register dll?
Example Tue Jun 10 19:02:17 2003 [Error]: ASO object class {7B7A13B3-8BB4-42A3- 8289-987C579797C2}did not implement IAfwAspectSystemObject Failed to create ASO. Forgot to register dll?
Reason This often occurs when a system extension is used, but not installed on the node from where the backup is taken. It can also happen if an update of a system extension has been installed, but not added to the system.
Solution Install and add all system extensions on the node from where the backup is taken. Make sure that the correct version of the system extension is installed.
Example Tue Jun 10 19:02:17 2003 [Error]: ASO object class {7B7A13B3-8BB4-42A3- 8289-987C579797C2}did not implement IAfwAspectSystemObject Failed to create ASO. Forgot to register dll?
Reason This often occurs when a system extension is used, but not installed on the node from where the backup is taken. It can also happen if an update of a system extension has been installed, but not added to the system.
Solution Install and add all system extensions on the node from where the backup is taken. Make sure that the correct version of the system extension is installed.
Add new comment