Accessing data from ABB AC 800M in ABB SCADA Vantage 5.1.1
We have ABB AC 800M PLC installed along with AC 800F RTU. Currently SCADA system is currently accessing data from AC 800 F RTU using SCADA Vantage 5.1.1 through ABB OPC server provided along with Control Builder F installation package.
How can i integrate the PLC 800M to existing SCADA system and able to view the data in SCADA Vantage 5.1.1?
How can i integrate the PLC 800M to existing SCADA system and able to view the data in SCADA Vantage 5.1.1?
Answers
- install the AC800M OPC server in the scada station .
- Other potion is to install a Modbus TCP card in the AC800M and take the data.
Add new comment