obsolete extensions after upgrade
After upgrade from 5.1 to 6.0 800xa I have some obsolete extensions e.g. VB stuff which could not be replaced:
Would you recommend to remove them? I get some errors in the full backup with these extension still in the system.
Would you recommend to remove them? I get some errors in the full backup with these extension still in the system.
Answers
VB extensions should be removed as per 2PAA111694-610 section 4.3. Make sure you don't have any VB aspects remaining in the system before doing so.
Regards
Regards
It is easier to remove the VB aspects before the upgrade. You can do this in an offline system. Once you restore the 5.1 system in V6 they are difficult to remove and do not backup properly either.
VBPG is not supported in SV6.0. It is mandatory to migrate VBPG to PG2 before Upgrading to SV6.0. The System 800xA VBPG Search Tool is used to find VBPG aspects in 800xA system that need to be migrated prior to a system upgrade to System 800xA 6.0.While System Restore Process Verify and review the message with missing System Extensions. Ignore the missing VB Graphics Extension.
Add new comment