800xA change the Default Drive for remote actions
The system is 800xA 6.0.3.2. On the second aspect server the Default Drive is still on C:\. Could I stop that machine and change the Default Drive to D:\ with the Configuration Wizard?
/Erik
/Erik
Voted best answer
Yes, use the System Configuration Console to move 800xA directories to different drives.
Assuming the server is redundant then there is no interruption to the system. Make sure the migration has finished COMPLETELY before doing anything else on the system. If you are migrating Basic History, ensure that the Service Performance Metrics show that "Percent Synchronised" reaches 100% on both servers.
Assuming the server is redundant then there is no interruption to the system. Make sure the migration has finished COMPLETELY before doing anything else on the system. If you are migrating Basic History, ensure that the Service Performance Metrics show that "Percent Synchronised" reaches 100% on both servers.
Add new comment