Asset optimization installation prerequisites
Asset optimization installation prerequisites
Answers
There is no specific prerequisites for Asset Optimization installation , as most of pre-requisites will be handled already while doing system setting prior running NPT. Mostly which include UAC enabling ,network sharing enabling , Firewall enabling , time zone, regional setting , IE Enhanced security turn off etc ....
Once all these are done , while installing AO using SCC , make sure IIS features are getting installed required by AO and this is also not manual step , IIS feature enabling is handle by System Installer.
In Sequence of AO Installation following actions will be done in SCC :
1. IIS feature enabling
2. Adding firewall ports / service rules
3. MATLAB Installtion
4. AO Build Installation
5. Post installation activities (Service creation ,start , etc ).
Then you are through to use it
Once all these are done , while installing AO using SCC , make sure IIS features are getting installed required by AO and this is also not manual step , IIS feature enabling is handle by System Installer.
In Sequence of AO Installation following actions will be done in SCC :
1. IIS feature enabling
2. Adding firewall ports / service rules
3. MATLAB Installtion
4. AO Build Installation
5. Post installation activities (Service creation ,start , etc ).
Then you are through to use it
Add new comment