Asset Optimization deployment stuck on Matlab Runtime
While deploying Asset Optimization, deployment stuck on Matlab Runtime. What would be the problem?
Voted best answer
Matlab installation usually takes times , However it will be good to see the installation logs to understand the problem
Answers
Solution:
1. End the Process of InstallMCR (Matlab Setup) from task manager while deployment is going on. It will show red mark on node due to failed deployment.
2. Install it manually from C:\ProgramData\ABB\800xA\MediaRepository\Applications\AssetOptimization\Install
MCR.exe
3. Go to the stopped deployment. Click Details à Manually resolveà Enter Reasonà Finish.
4. After that it will continue to install remaining things.
Add new comment