Is anybody try to install of 800xA 6.1 and QCS800xA 6.1 ??
As title says, is anybody try to test version of 800xA 6.1 and QCS800xA 6.1?
I set up this system ASCS combined system for demo but I got some weird situation.
In engineering workplace, service structure, system status viewer says all systems are ok.(Green color)
Even if every things are working well, Afw Service Connection Status are all not ok.(Red color)
I'll attach this pics as below you can easily understand what I'm talking about.


I set up this system ASCS combined system for demo but I got some weird situation.
In engineering workplace, service structure, system status viewer says all systems are ok.(Green color)
Even if every things are working well, Afw Service Connection Status are all not ok.(Red color)
I'll attach this pics as below you can easily understand what I'm talking about.


Answers
The Afw Service Connection Viewer (lower picture) is not meant to be used to display system status, rather connection status (primary/secondary network).
The System Status Viewer (upper picture) and the afwservicestatus.exe tool are the recommended sources for finding out system and service status.
A common reason to see the problem in the Afw Service Connection Viewer is an incorrect RNRP Network Filter setting (supplied when creating the system but can be viewed/changed using the traditional Configuration Wizard). Proper filter setting is required to ensure that the 800xA communication takes place over the correct network (in case there are more than one network available).
The System Status Viewer (upper picture) and the afwservicestatus.exe tool are the recommended sources for finding out system and service status.
A common reason to see the problem in the Afw Service Connection Viewer is an incorrect RNRP Network Filter setting (supplied when creating the system but can be viewed/changed using the traditional Configuration Wizard). Proper filter setting is required to ensure that the 800xA communication takes place over the correct network (in case there are more than one network available).
Add new comment