OPC server cant connect
Dear All,
i have issue with this OPC server that cant connect due to message "Failed to Connect to the controller. Duplicate application name.
please advise
Thank
BR
i have issue with this OPC server that cant connect due to message "Failed to Connect to the controller. Duplicate application name.
please advise
Thank
BR
Answers
ABB AC 800M?
I assume you noticed the warning about duplicate application name?
It is not possible to have multiple applications with the same name connected to the same AC 800M OPC Server. The default application name is Application_1 and may be reused multiple times of you have more than one controller, but not if you want to connect them to the same AC 800M OPC server.
If you have multiple applications & controllers to connect to a common AC 800M OPC server, ensure each application is given a unique name.
I assume you noticed the warning about duplicate application name?
It is not possible to have multiple applications with the same name connected to the same AC 800M OPC Server. The default application name is Application_1 and may be reused multiple times of you have more than one controller, but not if you want to connect them to the same AC 800M OPC server.
If you have multiple applications & controllers to connect to a common AC 800M OPC server, ensure each application is given a unique name.
Add new comment