Macafee Full scan in 800XA System
Is is recommended to do Mcafee full scan on the 800xa production system sheduled ?
Answers
Hi,
THis manual shows (section 7) what to exclude:
9ARD107543-005_J_en_System_800xA__Installing_and_Configuring_McAfee_ePO_server_
5.3
BR
THis manual shows (section 7) what to exclude:
9ARD107543-005_J_en_System_800xA__Installing_and_Configuring_McAfee_ePO_server_
5.3
BR
If it is a root kit scan then I think you need to do it and if you are a using it for the general purpose then scan it on
hi,
i run it 3 times a week. use the Randomise feature so that no two machines in your setup are doing a full scan at the same time - spread it out over a day.
In this day and age you have to consider full scanning.
dave
i run it 3 times a week. use the Randomise feature so that no two machines in your setup are doing a full scan at the same time - spread it out over a day.
In this day and age you have to consider full scanning.
dave
Add new comment