800xA for Freelance 6.0.3 windows firewall issue for basic history
Hello all,
we have a new 800xA installation to connect with freelance. During setup de windows firewall was turned on, so the installer could do the changes as required.
now we notice an issue with basic history, for example the data is not reachable from another client / server.
If we disable the windows firewall, everything worked.
Is there a specific firewall rule needed?
we have a new 800xA installation to connect with freelance. During setup de windows firewall was turned on, so the installer could do the changes as required.
now we notice an issue with basic history, for example the data is not reachable from another client / server.
If we disable the windows firewall, everything worked.
Is there a specific firewall rule needed?
Answers
It is better to perform a "Replace Node" from System Configuration Console for the particular Node , so that it adds the firewall exception while performing the installation.
For Replace Node follow manual "2PAA111708-600_en_System_800xA_Installation_Update_and_Upgrade_Getting_Started
"
For Replace Node follow manual "2PAA111708-600_en_System_800xA_Installation_Update_and_Upgrade_Getting_Started
"
Section 2 System Installation > Replacing a Node
Add new comment