CP600 vnc settings window
Answers
Greetings,
To enable the VNC client, open a project, go to project properties, this will open the project properties in the window to the left.

Now select the ‘Plug-in’ sub menu and set the VNC server option to True to enable it. This will ensure that this is downloaded into the target on the next download.
Also set ‘Developer Tools’ to True, this will give access to the advanced settings in the HMI’s context menu.
Hope it helps you.
To enable the VNC client, open a project, go to project properties, this will open the project properties in the window to the left.

Now select the ‘Plug-in’ sub menu and set the VNC server option to True to enable it. This will ensure that this is downloaded into the target on the next download.
Also set ‘Developer Tools’ to True, this will give access to the advanced settings in the HMI’s context menu.
Hope it helps you.
I solved the issue, i tried to download with the "download changes only" unchecked, but i faced an error, so i updated the packages using usb memory, and the issue was solved
Add new comment