AC500-ECO For Smart Panel
hey all
im working on a new project and am asked to Monitoring an 30 circuit breaker , these circuit breaker from abb which have built in Modbus
So what i need to do is :
1.draw single line diagram for the panel on an HMI , and when the user press on the Specific circuit breaker an pop up screen appears and it should hold all the information about the circuit breaker , until now its easy i can use CP610-ECO and make the drawing .
2.they need an data logger for each circuit breaker to log all the information for one year, so in that case what should i do ?
3.the panel far a way from the end user about three floor , so he want an HMI at the front of the panel , and he need to connect these HMI with His PC in the office to monitoring , in that case what to do ?
I need the best solution with the lowest price , please .
im working on a new project and am asked to Monitoring an 30 circuit breaker , these circuit breaker from abb which have built in Modbus
So what i need to do is :
1.draw single line diagram for the panel on an HMI , and when the user press on the Specific circuit breaker an pop up screen appears and it should hold all the information about the circuit breaker , until now its easy i can use CP610-ECO and make the drawing .
2.they need an data logger for each circuit breaker to log all the information for one year, so in that case what should i do ?
3.the panel far a way from the end user about three floor , so he want an HMI at the front of the panel , and he need to connect these HMI with His PC in the office to monitoring , in that case what to do ?
I need the best solution with the lowest price , please .
Answers
Greetings,
With CP600 series Operator Panels you can define datalogging. Both you can use internal or external memory for storing data.
By the way, if end user wants to see HMI on his PC, you can not use CP610-Eco, you need to use any CP600 model with WEB Server option. So end user easily connect HMI with his computer.
Hope it helps you.
With CP600 series Operator Panels you can define datalogging. Both you can use internal or external memory for storing data.
By the way, if end user wants to see HMI on his PC, you can not use CP610-Eco, you need to use any CP600 model with WEB Server option. So end user easily connect HMI with his computer.
Hope it helps you.
Add new comment