Digital Output Module DO562, Coil doesn't get on with NO variable. Please help,its urgent.
Hello Everyone, I am new to codesys programming and working project with PM554-ETH. I have created event based 4 tasks based on different process required by machine.
The problem I am facing now that Digital output does not get on when variable "TEST_IP" goes ON, but for NC contact "test1" it gets ON because of direct contact with power. I have attached image of ladder for better understanding.
Also, why when I force a input "TEST_IP", it show half blue rectangle and not like NC contact "test1"? is it the reason?
The problem I am facing now that Digital output does not get on when variable "TEST_IP" goes ON, but for NC contact "test1" it gets ON because of direct contact with power. I have attached image of ladder for better understanding.
Also, why when I force a input "TEST_IP", it show half blue rectangle and not like NC contact "test1"? is it the reason?
Answers
This question has not yet been answered.
by kstoilov
Hi,
Nothing attached in your post? Did you connect +24VDC to terminal 19 +L and 0VDC to terminal 20 M of DO562?
by Amey Pawaskar Rank: 1485 on 4/21/2019 2:06:47 AM | Like (0) | Report
Yes sir, I connected +24DC and 0VDC. But even when I do simulation in codesys, no coil in energizing in my program even when corresponding variable goes high.
by kstoilov
Hi,
I think in simulation mode the outputs will not energized. Try to write TRUE or BLINK output, connected to your output, download, go online and run the program
Add new comment