Panel pp845a restore
Voted best answer
Dear friend,
You can try factory restore with dip switches, but I don't think it will solve the problem with slow operation of the panel.
I faced the similar problem with slow operation of PP845 and it still exists, even after factory restore of the panel.
May be somebody else could share his experience here.
I guess the problem started when the project's size came close to the memory limit of the panel (too much trends for example).
I found one temporary solution - download the proect with checked "Force file delete in the terminal":
![]()

You can try factory restore with dip switches, but I don't think it will solve the problem with slow operation of the panel.
I faced the similar problem with slow operation of PP845 and it still exists, even after factory restore of the panel.
May be somebody else could share his experience here.
I guess the problem started when the project's size came close to the memory limit of the panel (too much trends for example).
I found one temporary solution - download the proect with checked "Force file delete in the terminal":
Answers
Hi,
if you have same version in factory value & in your Panel Builder project, then it should be fine to load the project right after factory reset (OBS remember to note down the settings before you do the factory reset).
If the versions are not the same, no problem again, after reset to factory setting, you only need to also upgrade the firmware to the newest version again (recommended due to bug fixes, etc). Then you can upload your panel builder project (check compatibility).
BR
if you have same version in factory value & in your Panel Builder project, then it should be fine to load the project right after factory reset (OBS remember to note down the settings before you do the factory reset).
If the versions are not the same, no problem again, after reset to factory setting, you only need to also upgrade the firmware to the newest version again (recommended due to bug fixes, etc). Then you can upload your panel builder project (check compatibility).
BR
Add new comment