System restore 800xa
Dear kstoilov;
We are working with pp845A, and my question is:
if we make a restore using dips, it’s possible if OPsys_b*.cab restored is an older version than the one which is installed now, probably updated been the panel in stock, won’t run the project which is charged nowadays?
Thank you so much!
We are working with pp845A, and my question is:
if we make a restore using dips, it’s possible if OPsys_b*.cab restored is an older version than the one which is installed now, probably updated been the panel in stock, won’t run the project which is charged nowadays?
Thank you so much!
Voted best answer
Hi,
I'm not quite sure if understood correctly your question. Is it the panel worked well before your restore?
What do you mean "..won’t run the project .."? No communication or the panel doesn't start itself?
Usually such a problems are not connected with the version of the firmware.
But you always could update the firmware too - look the following similar post:
https://forum-controlsystems.abb.com/...
Add new comment