Control Builder M - Control Module - Insert parameter from tree
Hi,
I create my own library with Data Types and Control Modules.
Test_Type - data type with 3x bool
test_ctrl_module - control module
I put my data type as 'param' and also few variables into control module.
In FBD I put "and" block and when I use:
"CTRL+T - Insert parameter from tree" I only see variables
"CTRL+J Insert parameter from list" I see variables + parameters
Why?
Kind Regards,
Voted best answer
Hmmm the difference should only be Insert from Tree / Insert From List.
But I think CTRL+J covers more than CTRL+T which only shows the variable tree available.
from manual : "Insert > Variable, Type, Attribute (or press CTRL+J) to access a list of possible data types."
But I think CTRL+J covers more than CTRL+T which only shows the variable tree available.
from manual : "Insert > Variable, Type, Attribute (or press CTRL+J) to access a list of possible data types."
Add new comment