hart configuration error
Hi,
I am using 800xa 6.0.3.2. I am configuring HART for KROHNE IFC100 rev4 electromagnetic flow meter.
I have extracted the DTM file through DLW and get no error. when I am going to configure the channel I am getting error as "Failed to create object! E_AFW_DTM_MISSING(0X8ABB4601) Object creation failed!!! the required DTM is either missing or not installed properly in this system.
now as per the release note 6.0.3.2 the issue has been resolved.
kindly suggest how to resolve the issue.
I am using 800xa 6.0.3.2. I am configuring HART for KROHNE IFC100 rev4 electromagnetic flow meter.
I have extracted the DTM file through DLW and get no error. when I am going to configure the channel I am getting error as "Failed to create object! E_AFW_DTM_MISSING(0X8ABB4601) Object creation failed!!! the required DTM is either missing or not installed properly in this system.
now as per the release note 6.0.3.2 the issue has been resolved.
kindly suggest how to resolve the issue.
Answers
Make sure that DTMs are installed in all 800xA nodes. Once installation completed in primary aspect server, open DLW in another node. This automatically synchronize objects from DLW server (primary aspect server). Once synchronization is over install all DTMs. The error message appeared due to missing DTM on that node.
Add new comment