RNRP shows paths "up" for primary connectivity server even if the network is down
Hi All,
In our system we have 2 sets of redundant Connectivity Server (CSAP,CSAS and CSBP,CSBS). During a redundancy check when we disconnected cables for CSAP and CSBP the RNRP monitor was showing both Paths "up" and this is only for the primary Connectivity Servers. The system is 800xA 5.1 FP3
Could some one please advise if its normal with the system or some settings needs to be carried out to resolve this issue.
Thanks
Miron
In our system we have 2 sets of redundant Connectivity Server (CSAP,CSAS and CSBP,CSBS). During a redundancy check when we disconnected cables for CSAP and CSBP the RNRP monitor was showing both Paths "up" and this is only for the primary Connectivity Servers. The system is 800xA 5.1 FP3
Could some one please advise if its normal with the system or some settings needs to be carried out to resolve this issue.
Thanks
Miron
Answers
Please restart RNRP (to clean up the logfile), reproduce the problem then attach a copy of C:\ProgramData\RnrpEvent.log
Add new comment