PM583-eth taking 100% Load
Dear,
We are using the PM583-eth with redundant system.
CPU is taking nearly 100% load and system many times break the communication with CHMI and PLC is Malfunctioning.
When i checked the program only 6.7% program memory used and 27% Retain memory used. And task is also define as per our standard.
Here I attached the backup file give the solution like plc will take load below 70%.
(COnvert attched file to .PRO)
.Txt>>>>>>.PRO
Answers
This question has not yet been answered.
Add new comment