Control builder plus 2.3v (AC500) software is not opening codesys.
This question is regarding control builder plus (version 2.3) of AC500 PLC. Also i am using windows 10 pro (64 bit) operating system of version 1803.
Now the problem is when i am clicking on the AC500 cpu symbol to open the codesys then a pop-up window is coming with an information which is " Retrieving the COM class factory for component with CLSID failed due to the following error: 80040154 class not registered". I have attached an image of this message.
This problem is also not giving any permission to save the project. In this condition what corrective steps i should follow? If any solution is there for this problem, then it will be helpful for me to fix this issue by following your suggestion. I am waiting for the valuable opinion.
BR.
Answers
Hi,
Officially Control Builder Plus 2,3V will not support windows 10 OS. Automation Builder 2.0 onwards supports Windows 10 OS.
Officially Control Builder Plus 2,3V will not support windows 10 OS. Automation Builder 2.0 onwards supports Windows 10 OS.
Hi
IMHO you can try one installation of Control Builder in a Virtual Machine (for example XP) inside your OS W10.
Regards
IMHO you can try one installation of Control Builder in a Virtual Machine (for example XP) inside your OS W10.
Regards
Add new comment