operator workplace is not opening automatically in operator login
Trying to login from a client (Operator Station) using the operator account, however the system is not automatically opening the workplace. Currently the system just logs in and can see all desktop with icons etc, . Is this a GPO related issue? Please advise on fixing this?
Voted best answer
What HMI? Freelance? Siemens? System 800xA?
Assuming the latter, have you made any configuration for automatic start of workplace?
If not... there will be no automatic start.
If yes... what did you do?
The procedure is different in 6.0 and onwards; below the topic you need to study in the user's guides if using 6.0 or 6.1.

Assuming the latter, have you made any configuration for automatic start of workplace?
If not... there will be no automatic start.
If yes... what did you do?
The procedure is different in 6.0 and onwards; below the topic you need to study in the user's guides if using 6.0 or 6.1.

Answers
Dear
Please refer the operator workplace configuration manual the page number from the 22 to 26 to start Auto workplace and to configure the full screen operator workplace.
Please refer the operator workplace configuration manual the page number from the 22 to 26 to start Auto workplace and to configure the full screen operator workplace.
Add new comment