IAC Communication between softcontrollers
I want to test communication between 2 applications (in the same project) by using 2 soft controllers. I used this type of communication in other applications before, but at that time I used only physical controllers. The 2 soft controllers are on the same PC, using the following addresses : 192.168.1.1:1 and 192.168.1.1:2.
I can download the applications whit out any errors , but I have no communication!
Is this possible or can I only use only physical controllers???
(I am using control builder 5.1.c)
I can download the applications whit out any errors , but I have no communication!
Is this possible or can I only use only physical controllers???
(I am using control builder 5.1.c)
Answers
I believe this is not supported in your version , only from version 6.0 on multiple soft controller properly work on the same pc. Try to run one of the soft controllers on another node for example virtual with VMware or similar.
Add new comment