DOC19 - AC450 Database Element Clock
Hi everyone,
Please, someone can share with me a documentation about the functionality of the DOC19 - AC450 Database Element Clock.
Thank you so much.
Please, someone can share with me a documentation about the functionality of the DOC19 - AC450 Database Element Clock.
Thank you so much.
Answers
DOC is a "Digital Output Calculated" - DOC19 is instance 19. So this makes no sense.
In AC450, the distribution of time is controlled by the "CLOCK_SYNCH" element. Check the AC450 Database Reference Manuals for Details. If you are using 800xA, there is also information about setting the Time Master in the 800xA for Advant Master manuals.

In AC450, the distribution of time is controlled by the "CLOCK_SYNCH" element. Check the AC450 Database Reference Manuals for Details. If you are using 800xA, there is also information about setting the Time Master in the 800xA for Advant Master manuals.

In additon to Rob's reply.
You will find most detailed information about clock sync settings and how it works, in the ABB Advant Masternet Users Guide
3BSE003839R301
In addition if you are using 800xA with AC400 connect, you will find additional settings needed in 800xA, in the 800xA with Ac400 connect documentation.
BR
JER
Add new comment