RTA Server connection timeout error
Trying to add & configure new PU410 RTA board to 400 connectivity server and getting RTA server connection timeout error. Able to add RTA board using Configuration wizard , but getting RTA Server connection timeout error while setting node & network number from RTA board control aspect.
Voted best answer
Do you have ping with PU410 RTA board? Are you using ethernet cross cable in direct connection from RTA to ethernet card of Connectivity server?
Is the PU410 driver installed successfully? There is DOS batch command file at installation media that can repeat installation of PU410 drivers, if necessary.
Is the PU410 driver installed successfully? There is DOS batch command file at installation media that can repeat installation of PU410 drivers, if necessary.
Add new comment