S100: LAN/BLK 0125 Device down alarm is coming in every five minute and after 10 sec it’s come to active state.
S100: LAN/BLK 0125 Device down alarm is coming in every five minute and after 10 sec it’s come to active state but IO card is healthy.
Answers
Hello.
With this information only, it's impossible to help.
You need to mention what controller, Is it MOD or Master ?
What HMI and SW version is used ?
What is the controller software version ? and what Hardware components are included in the I/O bus configuration ?
Which I/O board type is reported faulty? or Which I/O boards are used in the problem S100 I/O rack ?
Best Regards Jan-Erik
With this information only, it's impossible to help.
You need to mention what controller, Is it MOD or Master ?
What HMI and SW version is used ?
What is the controller software version ? and what Hardware components are included in the I/O bus configuration ?
Which I/O board type is reported faulty? or Which I/O boards are used in the problem S100 I/O rack ?
Best Regards Jan-Erik
Add new comment