Blinking Trends in Workplace
Good morning,
I'm using some "Primitive" Trends in the Overviews. Those trends brings the information from the LogConfig.
My problem starts when the information inside the Trend starts to Blinking without any sense. Sometimes I lose the whole history inside the trend and is needed to restart the Workplace.
I don't have this problem with the predefined trends which are using the template from the Library Structure (Top Right Screen in a 3 monitor setup).
Thanks in advance for your time.
I'm using some "Primitive" Trends in the Overviews. Those trends brings the information from the LogConfig.
My problem starts when the information inside the Trend starts to Blinking without any sense. Sometimes I lose the whole history inside the trend and is needed to restart the Workplace.
I don't have this problem with the predefined trends which are using the template from the Library Structure (Top Right Screen in a 3 monitor setup).
Thanks in advance for your time.
Answers
Enable setting “auto-scroll on ruler position “
has been provided in the general tab of the trend template
has been provided in the general tab of the trend template
by ATP
Which color you are selected for trend? static ?
by alxs9191 Rank: 1355 on 6/11/2019 7:36:18 AM | Like (0) | Report
I found the issue.
I was playing with the information displayed in the value with a simple "if" function. When I left the value as fixed .Out.Out or similar. Blinking problem goes away.
Thanks
Add new comment