Drive(ISU) is taking current without motor running or without command to drive to run, incomming ACB is tripping
INV and ISU ACS800-104-0580-7+E205+V991,
Answers
Hi!
This sounds like there may be an issue in the power stack of the drive.
But could be other issue also.
This sounds like there may be an issue in the power stack of the drive.
But could be other issue also.
Add new comment