branchement acs 880
bonjour , je veux adapter des variateurs ACS880 à un banc d'essai, la puissance des variateurs est de 5.5kw celle des moteurs est de 0.37kw, le problème c'est que dans ce cas l'application d'une commande DTC en vue relever la caractéristique mécanique n'est pas possible vue que le courant nominal moteur est inférieur au 1/6 de la sortie variateur (11A), caractéristique du moteur étoile 400v/ 1.2A triangle 230V/2.1 A
Answers
Hi
in the meantime I suggest you write in English, in order to allow all users to understand what you are talking about.
For your question, on a 0.37kW test equipment, you will certainly need to use a 0.55-kW ACS880.
A size too different and coarse will not allow you to have a good adjustment.
Alternatively, you should also consider using ACS380
Hope this help you
in the meantime I suggest you write in English, in order to allow all users to understand what you are talking about.
For your question, on a 0.37kW test equipment, you will certainly need to use a 0.55-kW ACS880.
A size too different and coarse will not allow you to have a good adjustment.
Alternatively, you should also consider using ACS380
Hope this help you
Add new comment