running Panel 800 Runtime on Windows 10 with a dongle
Hi Everyone,
I am installing the Panel 800 Runtime on Windows 10 with a dongle 4000. After successful installation i am not able to run. I am not sure if the 800 Runtime can work with windows 10.
Can everybody help me please.
Thanks
I am installing the Panel 800 Runtime on Windows 10 with a dongle 4000. After successful installation i am not able to run. I am not sure if the 800 Runtime can work with windows 10.
Can everybody help me please.
Thanks
Answers
Hi,
I can recommend to ask your ABB contact for some new updates, available for the product.
In the last available manual in the web site, I can see the requirements for Panel Builder 800 Runtime - Windows 7:
I can recommend to ask your ABB contact for some new updates, available for the product.
In the last available manual in the web site, I can see the requirements for Panel Builder 800 Runtime - Windows 7:
Source: 3BSE069489-603
Hi,
The new version Panel 800 V 6.1-0 supports both Windows 7 SP1, Windows 8.1 and Windows 10.
BR
ATP
The new version Panel 800 V 6.1-0 supports both Windows 7 SP1, Windows 8.1 and Windows 10.
BR
ATP
Hi,
Thanks for reply.
her are some screentcshots about the installation. But there is no symbol on the desktop to start.
Thanks for reply.
her are some screentcshots about the installation. But there is no symbol on the desktop to start.
Add new comment