What is the operating system that i should use to work with 800 XA 6.03?
Hi Geof, i hope you are having a good day. i wonder if you can help me with the question above. i cannot find a specific answer for my question.
i am going to use 800XA 6.03 in a new VM.
In the leaflet that comes with the installation files it mention Windows 8.1/Windows 2012 R2 but i think it is not up to date.
Thanks very much in advance
Manuel
i am going to use 800XA 6.03 in a new VM.
In the leaflet that comes with the installation files it mention Windows 8.1/Windows 2012 R2 but i think it is not up to date.
Thanks very much in advance
Manuel
Voted best answer
Please have a look at the System Guide (3BSE041434-600...). Depends if you have 6.0.3 or 6.0.3.1:
Keep in mind:
/Erik
Add new comment