800xA 5.0 sp2 Maintenance Backup Error- There is no valid restore node in the system
Thu Feb 21 18:04:07 2019 [Info] Starting backup...
Thu Feb 21 18:04:07 2019 [Error] There is no valid restore node in the system.
No node is running all the mandatory services
Thu Feb 21 18:04:07 2019 There is no valid restore node in the system.
No node is running all the mandatory services
Thu Feb 21 18:04:07 2019 [Error] There is no valid restore node in the system.
No node is running all the mandatory services
Thu Feb 21 18:04:07 2019 There is no valid restore node in the system.
No node is running all the mandatory services
Answers
Hi,
Verify that all service providers for Aspect Directory and FSD are running.
BR
ATP
Verify that all service providers for Aspect Directory and FSD are running.
BR
ATP
Hi all,
800xA 4.1 (2 out of 3 AS) maintenance backup is restored in 5.0 SP2 Rev E as a stand alone machine without domain
Pls find the attached screenshots for reference
800xA 4.1 (2 out of 3 AS) maintenance backup is restored in 5.0 SP2 Rev E as a stand alone machine without domain
Pls find the attached screenshots for reference
I am curious if you succeed to restore V4.1 full backup on version 5. Until now I thought restore target must be of the same version as original 800xa.
From maintenance manual:
If the restore runs in a different system than the backup was made in, a primary node
in the backup system must be remapped to the node your are running the restore on.
You remap a node by right-clicking the node in the restored system, and changing
the node name. See the figure below.

From maintenance manual:
If the restore runs in a different system than the backup was made in, a primary node
in the backup system must be remapped to the node your are running the restore on.
You remap a node by right-clicking the node in the restored system, and changing
the node name. See the figure below.

Hi All,
Thanks for the support, Now the backup is running. Engineering Base Service in service structure was causing the problem, Even it was in service Backup failed. I ran AfwEngineering.mdd located in "C:\Program Files\ABB Industrial IT\Operate IT\Process Portal A\mdd" folder and started the maintenance backup. Now working fine
Thanks for the support, Now the backup is running. Engineering Base Service in service structure was causing the problem, Even it was in service Backup failed. I ran AfwEngineering.mdd located in "C:\Program Files\ABB Industrial IT\Operate IT\Process Portal A\mdd" folder and started the maintenance backup. Now working fine
Add new comment