Upload project from Process Panel 245
Is it possible to upload a complete project from Process Panel 245? I found a retrieve button In the manual but im unsure If the whole project can be uploaded.
The original project Is missing.
The original project Is missing.
Voted best answer
Hello,
Yes, the complete project from PP245 can be uploaded (if the project itself is not password protected) and edited after that.
You can use Panel Builder 800 ver 5.1 or earlier, which supports PP245.
Yes, the complete project from PP245 can be uploaded (if the project itself is not password protected) and edited after that.
You can use Panel Builder 800 ver 5.1 or earlier, which supports PP245.
Add new comment