BROWSE 800XA TRENDS IN SMARTCLIENT
Hi,
Our 800xA DCS, IM Server, ASCS1, ASCS2, SmartClient all are in healthy running condition.
I need to Browse & display all my Trends of 800xA in SmartClient, in similar manner as we do in 800xA Operator Workplace.
Can somebody share the Settings/Procedure for same?
Following are the Versions of Softwares used:
800xA: 6.0-103
SmartClient: 2.2 RevC RU2b
Our 800xA DCS, IM Server, ASCS1, ASCS2, SmartClient all are in healthy running condition.
I need to Browse & display all my Trends of 800xA in SmartClient, in similar manner as we do in 800xA Operator Workplace.
Can somebody share the Settings/Procedure for same?
Following are the Versions of Softwares used:
800xA: 6.0-103
SmartClient: 2.2 RevC RU2b
Answers
Not sure what you mean by browsing. 800xA Trends can be "imported" into a Smart Client Panel using the Trend Browser.

These can be inserted as a New Tab according to the selections available when right-clicking on the desired Trend Page in 800xA. Panels, (Displays), in Smart Client are Tab based selections rather than a Menu as typically done in and 800xA OWP. Additionally, when an 800xA Trend is brought into Smart Client, the graphic portion with the traces is identical to the 800xA Trend, however, the elements around the graph are replaced by those of the Native Trend Panel of the Smart Client interface. All of the functionality of the 800xA Trend is available with the Smart Client Trend interface.
Additionally, if a PG2 Graphic is created in 800xA with multiple Trend elements, it to can be imported into a Smart Client Panel such as below.

Regards,
Geof Ledin

These can be inserted as a New Tab according to the selections available when right-clicking on the desired Trend Page in 800xA. Panels, (Displays), in Smart Client are Tab based selections rather than a Menu as typically done in and 800xA OWP. Additionally, when an 800xA Trend is brought into Smart Client, the graphic portion with the traces is identical to the 800xA Trend, however, the elements around the graph are replaced by those of the Native Trend Panel of the Smart Client interface. All of the functionality of the 800xA Trend is available with the Smart Client Trend interface.
Additionally, if a PG2 Graphic is created in 800xA with multiple Trend elements, it to can be imported into a Smart Client Panel such as below.

Regards,
Geof Ledin
Add new comment