PNSM Basic Computer Asset
Hi!
Is it possible to change Class of System Alarms from PNSM (fixed to 0)?
For instance System Alarms from Controller HW is configurable (default 9950).
BR
Is it possible to change Class of System Alarms from PNSM (fixed to 0)?
For instance System Alarms from Controller HW is configurable (default 9950).
BR
Voted best answer
Try using the (Event) Attribute Object Extension feature.
A 5-10 yrs old bulletin (who’s identity I cannot recall at the moment) gives example on usage. Search ABB Library for old alarm issues. I believe ”attribute” is part of the name.
A 5-10 yrs old bulletin (who’s identity I cannot recall at the moment) gives example on usage. Search ABB Library for old alarm issues. I believe ”attribute” is part of the name.
Add new comment