"MicroSCADA base system is not running. or not registered as a Terminal server application (MMC500_TS.CMD not run)
Hi, Ingo
I'm Guillermo londoño from ELECTROHUILA Colombia and I have SYS600 9.2 on W2003Server, I have the following error when I try to open the picn.exe application with remote desktop:
"MicroSCADA base system is not running.
or not registered as a Terminal server application (MMC500_TS.CMD not run). "
Thank you
I'm Guillermo londoño from ELECTROHUILA Colombia and I have SYS600 9.2 on W2003Server, I have the following error when I try to open the picn.exe application with remote desktop:
"MicroSCADA base system is not running.
or not registered as a Terminal server application (MMC500_TS.CMD not run). "
Thank you
Answers
Hi,
First stop the microscada services through the Microscada control panel and run the services called MMSC500_TS.CMD. This exe can find in the microscada SC folder. After running this , start the microscada from microscada control panel. Then you can run the Microscada with remote desktop.
BR
ATP
First stop the microscada services through the Microscada control panel and run the services called MMSC500_TS.CMD. This exe can find in the microscada SC folder. After running this , start the microscada from microscada control panel. Then you can run the Microscada with remote desktop.
BR
ATP
Add new comment