PCBA for soft starter PSE370 can be turn on soft starter PSE 300
Hello,
i hope you doing well
i have softstarter PSE300 and the PCBA for it are damage
can we replace it with PCBA but for other type (PCBA for PSE370)
Many thanks in advance for your help
regards,
i hope you doing well
i have softstarter PSE300 and the PCBA for it are damage
can we replace it with PCBA but for other type (PCBA for PSE370)
Many thanks in advance for your help
regards,
Voted best answer
Greetings,
Rated Operational Voltages are same for both softstarters, but Rated Operational Powers are different.
So it could happen some problem about current and power protection.
Rated Operational Voltages are same for both softstarters, but Rated Operational Powers are different.
So it could happen some problem about current and power protection.
Answers
Hi,
If you are talking about the cooling fan (1SFA899215R1080) according to the spare parts catalog ( 1SFC132013C0201) it is the same for all softstarters PSE210 ... PSE370.
So I think you can replace it without problem.
If you are talking about the cooling fan (1SFA899215R1080) according to the spare parts catalog ( 1SFC132013C0201) it is the same for all softstarters PSE210 ... PSE370.
So I think you can replace it without problem.
Add new comment