where does the VB Graphics migration tool store it's configuration data
Does anybody know where the VB Graphics migration tool stores the data about the mapping of the aspects and the properties. I have to migrate graphics of several 800xA systems which are based on the same libraries. The mappings are quite extensive as we have combined several graphic elements in to one element e.g. a motor, a pump, a compressor graphic are now combined into one element with an input property to show the right picture. I would like to save or export the configuration of the VB graphics migration tool to reuse it.
Answers
To answer myself: they are stored in the PG2 graphic element. So if you put the elements in an extension library and export that you can import them back to you control code library on a different system.
Add new comment