Change active service in Afw Connection Status
Hi
I'm on one engineering station and logged in as 800xAService. and the system is 800xA 6.0
When i look at ”Afw Service Connection Status” on one client I can see for example that I have “Event Collector” on CS1 active and “Event Collector” on CS2 not active.
I can’t change from “Event Collector CS1” to “Event Collector CS2”. That because I cant choose “Edit” in the menu.
In other system, 5.1, I had that option.
Now I am on a system 6.0 and this option doesn’t appear.
Is it gone In version 6.0?
/anders
Answers
I believe "edit" mode need elevation; the tray icon launches the service connection viewer in non-elevated mode and no code has been added to "elevate" on demand.
Try finding the .exe in the well-known folder of 800xA executables, right click it and "Run as administrator..."
by kstoilov
Basically you don't have to log-on with Service account, better try when log-on as administrator
Add new comment