Function Block not deleted from Declaration Pane when deleted in FBD Editor
We have upgraded an 800xA System from 5.0 to 6.0 where all the Code is done in Single Control Modules with FBD Editor. Now the behavior of Control Builder M seems to have changed, on deleting Function Blocks the Entry in the Table (Declaration Pane) even if the Function Block is not referenced anywhere else. This always needs to be done manually... or the entries remain and there is the warning 1542 "function block xy is not called".
In 5.0 this has worked correctly - on deleting the Function Block in the Code Pane, the Entry in Declaration Pane is removed as well.
Can this behavior be corrected by some setting or System Variable?
In 5.0 this has worked correctly - on deleting the Function Block in the Code Pane, the Entry in Declaration Pane is removed as well.
Can this behavior be corrected by some setting or System Variable?
Voted best answer
Greetings,
Same situation exist for v5.1 also.
You need to delete all not called Function Blocks or Control Modules manually.
https://forum-controlsystems.abb.com/...
Hope it helps you.
Same situation exist for v5.1 also.
You need to delete all not called Function Blocks or Control Modules manually.
https://forum-controlsystems.abb.com/...
Hope it helps you.
Add new comment