OPC Server goes down everytime after download - 800xA 6.0.3
Hello,
I face one issue in 800xA system 6.0.3 AC800M connect.
System is up & running; CBM is online; OPC server configuration shows yellow smiley (with soft controller).
However if i make any changes and download CBM again, opc server communication goes red. Everytime i have to browse application specific files .ctdxml, .cdoxml & .rrxml from Compiler Output folder.
I have made the Autoload configuration as well. Still every time I'm browsing these files. How to avoid browsing these files everytime after download? Please recommend.
Thanks
Answers
There are Two common reasons the OPC Server cannot find the domain files: 1.Wrong Service Account, (no privileges to access aspect directory or Shared network disk) 800xA . 2.Wrong System connection.

open the System dialog box by selecting Settings > System Connection... from the OPC Server Configuration Panel.

open the System dialog box by selecting Settings > System Connection... from the OPC Server Configuration Panel.
Add new comment