PM583-ETH does not communicate ethernet port.
How can I check that the ethernet port of PM583-ETH is enabled or that it is in good condition ?. I can not access from software to PLC. Do I need to enable this port from the PLC keyboard?
I can access through the serial port, I could not by ethernet port. PLC PM583-ETH A9 and base TB521-ETH B2
I can access through the serial port, I could not by ethernet port. PLC PM583-ETH A9 and base TB521-ETH B2
Answers
Hi
Have you test the IP config utility?
Otherwise, you could simply try, if you know the IP address of the cpu, to use the command "ping" from your PC the console mode ... to know the IP address of the CPU you have to check it from the display according to the instructions for access commands from display.
Hope this help you
Have you test the IP config utility?
Otherwise, you could simply try, if you know the IP address of the cpu, to use the command "ping" from your PC the console mode ... to know the IP address of the CPU you have to check it from the display according to the instructions for access commands from display.
Hope this help you
Add new comment