SIL2 to nonSIL communication variables
Hello,
I try to establish communication between applications on different controllers. Please see attached file for full information
I try to establish communication between applications on different controllers. Please see attached file for full information
Answers
Greetings,
Could you please attach the file?
Could you please attach the file?
Hai dear,
To establish the communication between the non sil to sil application or one controller to another controller you should have to keep the expect sil as non sil in both communication variable tab, in both projects and unique ID should be same. Even you set above points it will give error in the SIL application, for that you navigate to the right click on project tree<settings<compilier switches <then non sil communication variable set as warning in the SIL 3. I hope you understand this.
To establish the communication between the non sil to sil application or one controller to another controller you should have to keep the expect sil as non sil in both communication variable tab, in both projects and unique ID should be same. Even you set above points it will give error in the SIL application, for that you navigate to the right click on project tree<settings<compilier switches <then non sil communication variable set as warning in the SIL 3. I hope you understand this.
Add new comment