CHMI 6.0 Implementation (Direct file reading or DB required)
Hello everyone!
I am implementing a new project using CHMI 6.0. I don't have enough knowledge about this application, and so I have some questions hoping anyone could help:
1st: Can this scada read the txt. files directly through a script or other function?
2nd: If we use a DB SQL Express can the scada communicate w/ the BD using ODBC?
3rd: If none of the 2 options given before are available, is there any other suggestion that I should consider using?
I am implementing a new project using CHMI 6.0. I don't have enough knowledge about this application, and so I have some questions hoping anyone could help:
1st: Can this scada read the txt. files directly through a script or other function?
2nd: If we use a DB SQL Express can the scada communicate w/ the BD using ODBC?
3rd: If none of the 2 options given before are available, is there any other suggestion that I should consider using?
Answers
This question has not yet been answered.
Add new comment