automation builder 2.0 - missing export/import tabs
Refer to your doc page 14, no import/export features appeared: I first installed the software on a win 10 home. When open a PLC project seems ok until I tried to export the symbol file.
I clicked on the project tree - tab: application, I expected to see the export/import features to export the symbol file.
These import/export options are missing from the system.
Refer to your doc page 14, after I click on the application tab, the import/export features are missing from the menu. That is the problem.
I then upgraded the computer to a win 10 pro, and installed the same software. The same problem persisted.
Anythink I should check and do?
I clicked on the project tree - tab: application, I expected to see the export/import features to export the symbol file.
These import/export options are missing from the system.
Refer to your doc page 14, after I click on the application tab, the import/export features are missing from the menu. That is the problem.
I then upgraded the computer to a win 10 pro, and installed the same software. The same problem persisted.
Anythink I should check and do?
Answers
This question has not yet been answered.
Add new comment