Display issues with Codesys V2.3
Hello,
I have an issue with Codesys V2.3. When I open the program, part of the UI looks good, but part of it is unreadably small or badly positioned. I included a sample picture. I had the same issue with Automation Builder (but nothing else), which I was able to resolve by using the "Override high DPI scaling behavior" option in Properties/Compatibility in the context menu of the program icon. However, this method does not work with Codesys. I tried other compatibility options as well but couldn't find a solution.
What can I do about it?

I have an issue with Codesys V2.3. When I open the program, part of the UI looks good, but part of it is unreadably small or badly positioned. I included a sample picture. I had the same issue with Automation Builder (but nothing else), which I was able to resolve by using the "Override high DPI scaling behavior" option in Properties/Compatibility in the context menu of the program icon. However, this method does not work with Codesys. I tried other compatibility options as well but couldn't find a solution.
What can I do about it?

Answers
Hi
are you using Codesys in the Automation Builder suite? Which version?
With other programm - Codesys version or Automation Builder - do you have the same problem?
IMHO you can solve with one new installation of the entire Automation Builder suite.
Hope this help you
are you using Codesys in the Automation Builder suite? Which version?
With other programm - Codesys version or Automation Builder - do you have the same problem?
IMHO you can solve with one new installation of the entire Automation Builder suite.
Hope this help you
Add new comment