Can a TC630 connect with a TC514 on the Optic Port
Is it possible to connect a TC630 to a TC514? Both have an optical link, but none of the documentation shows this combination, only a TC630 connecting to a TC630 or a TC514 connecting to a TC514. Has anyone tried this.
Reason for the query is that we are upgrading some APCs (AF100 coax over fibre) with AC800 (AF100 TWP) and there is an existing TC630-TC630 link.
Reason for the query is that we are upgrading some APCs (AF100 coax over fibre) with AC800 (AF100 TWP) and there is an existing TC630-TC630 link.
Answers
Hello.
This should be possible.
I have seen this configuration before, where the customer had one TC625 and one TC630 at the AC450 controller side and then fiber to TC514V2 which was used in the remote (field side).
Best Regards
Jan-Erik
Add new comment